How can we help you today?
How to reset wiser2 back to factory default?
There are several reasons why you may wish to restart or reset the Wiser 2. If the unit is not communicating properly, a restart (turning power on and off)might be all that is required but for a full factory reset.
NOTE: Performing a Factory "Full" Reset will wipe any programming of the unit and reset the ip addressing to DHCP and the username and password to default - "default"
If a Factory Reset is required follow these steps:
(1) Power OFF the Wiser 2
(2) Press and hold the reset button
(3) While the button is pressed, apply power to Wiser 2
(4) After the required time, release the button and allow the Wiser 2 to reboot.
Released for:Schneider Electric Australia
Explore more
Product:
Explore more
Product: