{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
How to set up ATV320 for Speed Reference via Modbus and Start/Stop via Terminals ?

Step 1
For Modbus Serial , FR1 à Integrated Modbus
And for Modbus TCP , FR1 à Com Card

Step 2
To separate the Start/Stop command to the speed reference , please change control mode configuration CHCF to Separate/IO profile,
CHCF à Separate (sequential method)
CHCF à I/O Profile (allows to write to the command register of the drives in bits)

Step 3
Please check CD1 is set to terminals,
CD1 à Terminals (by default)

ATV320 Programming Manual and ATV320 Modbus Manual is attached for reference.

ATV320 .png

Schneider Electric Australia

Attachment(s)
ATV320_Programming_Manual_EN_NVE41295_03.pdf [2.5 MB]
ATV320_Modbus_manual_EN_NVE41308_01.pdf [4.48 MB]
Explore more
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: