{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
What is the power of the wireless transmitters such as the ZBRN1 and PowerTag Link ?

The maximum isotopically radiated power of the ZBRN1 transmitter are :

  • With its internal antenna: 9.8 dBm (10 mW)
  • With a ZBRA2 external antenna: 4.8dBm (3.02 mW)

Schneider Electric Australia

Explore more
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: