{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
Which Ethernet modules or PLCs is the TCSEGPA23F14F PRM master compatible with?
The TCSEGPA23F14F can be used with the M580 CPU and NOC modules as well as the NOE module for the M340 CPU. For the Premium PLC, it can be used with an ETY module or embedded CPU port. Note, it cannot be used with a TSXETC101.

Schneider Electric Australia

Explore more
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: