{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

How can we help you today?

What Class is Wiser2/SLHC (5200WHC22) Network Support?

Unfortunately, to be able to disable the remote connection for Projector Control Wiser 2 only supports class C network.

A class C network would have a subnet mask of 255.255. 255.0, which means that 24 bits are used for the network. In CIDR notation, this is designated by a /24 following the IP address


Schneider Electric Australia

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: