How can we help you today?
"Cannot create task" error during startup of Runtime Project in PowerScada
Issue
Getting "Cannot create task" error during startup of Runtime Project and I/O Server stops.
Product Line
EcoStruxure Power Operation
Resolution
This is caused by duplicate IO Device names. This can be verified by reviewing the IO Device names in Units database, if duplicates exist either rename them or delete the unwanted device.
Released for:Schneider Electric Australia
Explore more
Range:
Explore more
Range: