{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
Does Vijeo Designer v6.3 support Windows 11?
Issue:
OS compatible with Vijeo Designer 6.3

Product Line:
Vijeo Designer 6.3

Environment:
Windows 10, Windows 11

Resolution:
Vijeo Designer 6.3 is now validated in Windows 10 Pro and Windows 11. It is officially supported by these OS. At the moment it is not validated with any Windows Server.

Schneider Electric Australia