How can we help you today?
Vijeo Designer Runtime Application Has Halted: IVM.dlm:Koohi.cpp
The error message "Vijeo Designer Runtime Application Has Halted: IVM.dlm:Koohi.cpp" indicates that there was a problem with the Vijeo Designer Runtime application. Specifically, the error occurred in the "Koohi.cpp" file within the "IVM.dlm" module.
To fix this error, it is recommended to apply the latest hotfix that is provided in the attachment. Hotfixes are updates released by the software developer to address known issues, including bugs and errors. Installing the latest hotfix can often resolve the specific issue encountered in the "Koohi.cpp" file.
Additionally, it is worth noting that using an outdated version of Vijeo Designer could contribute to the occurrence of this error. Software updates and newer versions often include bug fixes, enhancements, and performance improvements. Therefore, it is advisable to ensure that you are using the most recent version of Vijeo Designer to minimize the occurrence of such errors.