{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
Harmony HMI "Your computer is low on memory" Error
From the Task Manager, check the memory usage of each application. If there is an application with an excessive usage, try to close it.

Also, it is possible to set up Virtual memory as well.
  1. Go to Control Panel->View advanced system settings (you can just type it from the Start bar).
Windows setting
  1. Then in the System Properties dialog, go to the Advanced Tab.
  2. Under Performance, click on the Settings… button.
  3. In Performance Options dialog, go to the Advanced Tab.
  4. Under Virtual Memory, click on the Change… button.
  5. In the Virtual Memory dialog, untick the “Automatically manage paging file size for all drives” checkbox if it is ticked.
  6. Select C:\ from the list.
  7. Select “Custom size”.
  8. Assign 4GB (4096MB)
  9. Click OK.

Steps

Schneider Electric Australia

Harmony HMI "Your computer is low on memory" Error
From the Task Manager, check the memory usage of each application. If there is an application with an excessive usage, try to close it.
 
Also, it is possible to set up Virtual memory as well. 
 
  1. Go to Control Panel->View advanced system settings (you can just type it from the Start bar).
Windows setting
  1.  Then in the System Properties dialog, go to the Advanced Tab.
  2. Under Performance, click on the Settings… button.
  3. In Performance Options dialog, go to the Advanced Tab.
  4. Under Virtual Memory, click on the Change… button.
  5. In the Virtual Memory dialog, untick the “Automatically manage paging file size for all drives” checkbox if it is ticked.
  6. Select C:\ from the list.
  7. Select “Custom size”.
  8. Assign 4GB (4096MB)
  9. Click OK.

Steps

Schneider Electric Australia

Explore more
Range:
Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
Explore more
Range:
move-arrow-top