{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
How to declare MTZ MCH in EPC
Issue:

How to declare MTZ MCH in EPC

Product Line:

EPC

Environment:

MTZ

Resolution:


Please refer to the FAQ video which can help you to declare and configure MTZ MCH motor gear, MCH will not recognize the MCH automatically and the purpose to configure the MCH is to record the operation time of the MCH, Micrologic will alarm customer to replace if the MCH operation time closes to its life span.

You may please refer to the MCH instruction sheet (attached) for how to install MCH, always check for the latest instruction sheet from SE website.


Schneider Electric Australia

Attachment(s)
files.pdf [3.3 MB]