{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
Is there an isolated relay output card for the x80 I/O?

Yes the BMXDRA0815 is a 16 point isolated relay card.

BMXDRA0815 - discrete output module, Modicon X80, 8 NO relay outputs, 24 to 240V AC, 24 to 125V DC | Schneider Electric Australia (se.com)

Schneider Electric Australia

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: