{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

How can we help you today?

Where to download the C-Bus PICED 4.15.2?

Where to download the C-Bus PICED 4.15.2?

Release Date: 05/03/2024
Version: V4.15.2
Reference: PICED-V4.15.2
C-Gate: 3.3.0 (build 1825)
Operating systems: Windows 11 Professional (64-bit), Windows 10 Professional (64-bit), Windows 10 Enterprise (64-bit), Windows 10, Windows 8, Windows 7

What’s New
C-Bus Home Controller Project NTP Servers
The default NTP server URLs in the Project Details Wizard > C-Bus Controller > NTP project settings have been modified to:
• 0.schneider.pool.ntp.org
• 1.schneider.pool.ntp.org
• 2.schneider.pool.ntp.org
• 3.schneider.pool.ntp.org

Fixes
• Fixed an issue where the password security routines were generating incorrectly encoded values in a specific workflow
• Fixed an issue where, after transferring the project from a Wiser 2 or C-Bus Home Controller device, the project file was not restored correctly
• Adjusted the Transfer Utility to better recognise remote Wiser 2 and C-Bus Home Controller devices with firmware that does not report the full version
• Fixed an issue in the Transfer Utility with connecting to a local Wiser 2 / C-Bus Home Controller device after having connected to a remote device
• Updated information regarding encrypted communications with a Wiser 2 / C-Bus Home Controller device
• Fixed an issue in the Transfer Utility with determining the security level required by the device when connecting remotely
• Fixed an issue in the Transfer Utility with transferring a project from a remotely connected device


Link to download C-Bus PICED 4.15.2
https://www.se.com/au/en/download/document/PICED-V4.15.2/
or
https://www.se.com/au/en/product-range/2216-spacelogic-cbus-home-automation-system/?parent-subcategory-id=88010&filter=business-5-residential-and-small-business#software-and-firmware

Schneider Electric Australia

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: