How can we help you today?
PME - Client Access License Features
Issue
What are the features of the Client Access License
Product Line
EcoStruxure Power Monitoring Expert
Resolution
From the PME user guide - https://product-help.schneider-electric.com/EcoStruxure-Power-Monitoring-Expert-2023/content/2_planning/licensing/licensingoverview.htm
Client Access License
This is a required license. It allow access to Web Applications.
- Client Access licenses are assigned to users.
- Each user needs their own Client Access license.
- A Client Access license is assigned and bound to a new user when they first log into the PME web applications.
- The supervisor account also needs a Client Access license.
- To free up an assigned Client Access license, the user must be deleted in PME.
NOTE: An unlimited Client Access license is available that includes unlimited web application use.
NOTE: Management Console does not require a license.
Released for:Schneider Electric Australia
Explore more
Product:
Range:
Explore more
Product:
Range: