Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.

Arc Fault Detection Devices help to reduce the risk of electrical fires

Broken wires, loose connections, crushed cables, worn insulation can all cause hidden arc faults in electrical circuits, which if left undetected, can erupt into flames in just seconds. AFDDs (also known as Arc Fault circuit interrupter in some countries) isolate the faulty circuit the moment an arc fault is detected.

Hidden Danger

An arc fault is not always easy to see, since it can occur in hidden places such as damaged cables, inside walls, a loose connection in a hidden junction box, or socket outlets.

Arc fault fires: how they start

Very localised phenomena can cause an electrical fire. Check out this video to learn more about different type of arc faults and how they start.
 

What is an Arc Fault Detection Device?

An AFDD is a circuit breaker that automatically cuts the electricity supply when it detects an arc fault in a circuit. By immediately cutting off the electricity supply, AFDDs help to prevent arc faults from reaching temperatures where fires can break out.

Schneider Electric AFDDs comply with IEC 62606, a new international standard covering product safety and performance.

Acti9 iArc

Arc Fault Detection device only

Acti9 iDPN H VigiArc

Arc Fault detection with circuit breaker and RCCB function

Where to use AFDDs?

Since 2019, AS/NZS 3000:2018 recommends the use of AFDDs to protect against arc faults in final sub circuits in the following applications:

Escalated Risk

Arc fault risk is expected to be higher for power circuits (connected to socket outlets) due to following reasons:
  • Arcing in extension boards.
  • Damage to cables plugged into socket outlets behind furniture like bedsides or sofas.
  • Damage to extension leads due to bending around corners or trapping under furniture.
  • Damage to plugged cables due to temperature variation, ultraviolet rays, vibrations, humidity, and rodents in outdoor environment.
Therefore, we highly recommend using AFDD for power circuits as a minimum.

Can other protective devices replace AFDDs?

Thanks to smoke detectors, building occupants get alerted to the presence of smoke AFTER a fire has started. Early detection helps occupants to evacuate before a fire gets too big. Unfortunately, smoke alarm can’t prevent fires. Lower mobility of people due to age, disability, location might not provide enough time to evacuate. AFDDs are designed to help PREVENT an electrical fire due to arc faults from starting.
Compact and easy to install, AFDDs fit into electrical switchboards, alongside other protective equipment. They cannot be replaced by any other protective devices like miniature circuit breakers (MCBs), surge protection devices (SPDs), or residual current devices (RCDs). While these protect against specific electrical hazards, they are not designed to detect arc faults.

Learn how AFDDs help protect buildings

Discover new advancements in the field of arc fault detection and identify the critical application for arc fault breakers to enhance home safety in our complimentary guide.
Download White Paper opens in new window

How to get support from your electrician

Schneider Electric AFDDs

Contact your electrician and find out more about the Schneider Electric AFDDs.

Electrical system safety

When designing a new construction site, consult with experts who can analyze electrical system safety requirements and can validate the design.

Audit existing sites

For renovation projects, audit existing sites to determine the level of deterioration in the core wiring systems.

Trade

Learn more about installing AFDD and diagnosing cause of tripping for your customers.
Read More opens in new window

Frequently Asked Questions

Need more information about ArcFault Detection Devices?

ArcFault FAQs opens in new window

Need help?

Product Selector

Quickly and easily find the right products and accessories for your applications.

Get a Quote

Start your sales inquiry online and an expert will connect with you.

Where to buy?

Easily find the nearest Schneider Electric distributor in your location.

Help Centre

Find support resources for all your needs, in one place.

Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.