{}

Nos marques

Bienvenue sur le site Web de Schneider Electric

Bienvenue sur notre site Web.

Consulter notre FAQ

How do you address a Modbus Coil boolean tag in a EcoStruxure Machine Expert controller?

Issue
How do you declare a symbol in EcoStruxure Machine Expert or SoMchine in a PLC with a Modbus Coil boolean 0x or %M address?

Product Line
Modicon M238, LMC058, M258, M241, M251, M262, PacDrive 3, EcoStruxure Machine Expert, SoMachine

Environment
PLC Configuration software in Windows 10

Cause
There are no Modbus Coil (0x notation or %M) boolean address space in SoMachine / EcoStruxure Machine Expert PLCs.
Only Holding Registers exist in SoMachine / EcoStruxure Machine Expert PLCs.

Addressing of the Double Words, Words, Bytes, and Bits are described in this table (which applies for all M2xx Logic PLCs supported in SoMachine / EcoStruxure Machine Expert):
Holding Register memory addressing table

Resolution
You will need to declare bits within a BYTE of a Holding Register using the notation %MX<y>.<z>
<y> is the Byte offset starting at 0
<z> is the Bit offset from 0 to 7 of the <y>th byte

Here is an example of a Variable declaration of 4 bits within a single Holding Register:
VAR
    bVar1 AT %MX200.0: BOOL;
    bVar2 AT %MX200.7: BOOL;
    bVar3 AT %MX201.0: BOOL;
    bVar4 AT %MX201.7: BOOL;
END_VAR

bVar1 is the 0th bit of %MW100 (%MW100.0)
bVar2 is the 7th bit of %MW100 (%MW100.7)
bVar3 is the 8th bit of %MW100 (%MW100.8)
bVar4 is the 16th bit of %MW100 (%MW100.15)

Notice that there are 2 Byte addresses per 1 Holding Register Word.

Schneider Electric Belgium

En savoir plus
Gamme :
En savoir plus
Gamme :