Easergy P5 Communication: Can I use both IEC61850 together with a different Ethernet protocol like DNP over Ethernet or Modbus TCP at the same time?Yes, Easergy P5 relays support the use of two (2) protocols simultaneously, in the same communication port or in 2 different ports.
Publié pour:Schneider Electric Belgium