{}

Nos marques

Bienvenue sur le site Web de Schneider Electric

Bienvenue sur notre site Web.
Consulter notre FAQ
What is the default password for EcoStruxure Panel Server?

Issue

The user may need to know what the EcoStruxure Panel Server password is during the initial installation.

Product Line

EcoStruxure Panel Server (The 3 models of EcoStruxure Panel Server are Universal (PAS600 series), Advanced (PAS800 series), and Entry (PAS400, available later).

Environment

Installation – Configuration

Cause

EcoStruxure Panel Server first installation.

Resolution

The EcoStruxure Panel Server (PAS) does not have a default password during the initial installation but can be created by the customer the first time connecting it. Log in using the default username SecurityAdmin. Set a password, following the requirements (see Password Requirements, page 139). So, the PAS doesn’t require any credential (Username and Password) when accessing locally, but when dealing with Data publication in the cloud for example or Security purpose the password is mandatory. All the PAS levels (Entry, Universal and Advanced) have the following default administrator account “SecurityAdmin” (See user guide under management section). The following warnings will appear if the SecirityAdmin password is not setup.

Figure 1: Initial commissioning

PAS - Initial commissioning

This can be initially done using:

• EcoStruxure Power Commission software. Download here.

• Or the home page of EcoStruxure Panel Server webpages

The EcoStruxure Panel Server documentation is in this link FAQ000239552

If you can’t log into webpages due to lost or forgotten password, see the user guide under “Resetting to Factory settings” for instruction.


Schneider Electric Belgium

En savoir plus
Produit :
Gamme :
Articles utiles
En savoir plus
Produit :
Gamme :