Our Spacial S3D, CRN, SBM, SF and SM enclosures and cubicles as weel as the PanelSet SFN cubicles can be used under below mentioned T°:
Conditions for use: Ambient air temperature for outdoor or indoor installations: -25 to +40 ºC.
Atmospheric conditions for outdoor installations: The humidity may temporarily reach 100% at a temperature of 25 ºC.