{}

Onze merken

Impact-Company-Logo-English Black-01-177x54

Welkom op de website van Schneider Electric

Welkom op onze website.
Populaire vragen (FAQ's) zoeken
Is there a 9001 KA contact block that is rated 6A at 125VDC?
Issue:
9001KA contact rating

Product Line:
9001 Type K Heavy Duty Operators

Environment:
30 mm Push Buttons

Resolution:
No., the 9001KA contact blocks have a maximum of 2.5A continuous at 125VDC.

Schneider Electric Belgium

Ontdek meer
Productfamilie
Mogelijk nuttige artikelen
Ontdek meer
Productfamilie