Issue:
Accuracy of the Timers in ProWorx32
Product Line:
ProWorx32
Resolution:
The accuracy of a timer is +/- one incremental value or the scan time which ever is greater. So a T.01 timer has an accuracy of +/- 0.01 seconds provided that the scan time is less than 0.01 seconds.
Gepubliceerd voor:Schneider Electric Belgium