Populaire vragen (FAQ's) zoeken
What pin out can be used for Momentum RJ45 to RJ45 RS232 Modbus communications?
Cabling scheme for the RJ-45-(8x8) to RJ-45-(8x8) (null modem);
This pin out is to be used for Momentum to Momentum RS232 connection only (XMIT/XXMIT).
Legacy KB System (APS) Data: RESL192681 V1.0, Originally authored by RoAl on 09/03/2008, Last Edited by RoAl on 09/03/2008
Related ranges: Modicon Momentum
Gepubliceerd voor:Schneider Electric Belgium
Ontdek meer
Productfamilie
Ontdek meer
Productfamilie