Issue
Register list for Modbus communication
Product Line
PM5110, PM5330, PM5340, PM5560, PM5563, PM56xx, PM57xx
Environment
Power Meter Communications Modbus Register List
Cause
PM5000 series register list is needed for Modbus communication
Resolution
See the attached documents for Register List.
There are 2 files. One for the PM5100 and PM5300 series and the other file is for the PM5500, PM5600, and the PM5700 series.
Gepubliceerd voor: Schneider Electric Belgium