{}

Onze merken

Impact-Company-Logo-English Black-01-177x54

Welkom op de website van Schneider Electric

Welkom op onze website.
Populaire vragen (FAQ's) zoeken
What cable is used to communicate via Modbus TCP/IP (USB Equipment) between the M340 to HMIGTO?
Issue:
Looking for assistance on how to connect the M340 PLC to a Magelis HMI in order to communicate over Modbus TCP/IP USB Equipment as defined in Vijeo Designer.

Product Line:
Vijeo Designer, Magelis HMI, M340

Resolution:
The BMX-XCA-USBH018 is the cable to communicate by Modbus TCP/IP via USB between the M340 and the HMIGTO5310.

The mini-USB end plugs into the M340 and the standard USB end plugs into the HMIGTO

Schneider Electric Belgium

Ontdek meer
Productfamilie
Mogelijk nuttige artikelen
Ontdek meer
Productfamilie