Does BlokSeT/Okken MCC offer comply with ANSI/NEMA MCC-Switchgear Standard?No BlokSeT/Okken switchboard is designed as per the IEC standards IEC61439- 1 & 2. It does not comply with ANSI/NEMA MCC - Switchgear standard.
Gepubliceerd voor:Schneider Electric Belgium