undefined [object Object]
{}

Onze merken

Welkom op de website van Schneider Electric

Welkom op onze website.
Hoe kunnen wij u vandaag helpen?
The Write_Var instruction requires an Array of INT for the EMIS input. How do I move UINT values to a remote device?
You simply need to convert the UINT to INT with the UINT_TO_INT block and move the result to the EMIS array.
If the receiving device does not automatically see the data as UINT you would need to use the INT_TO_UINT block
to see the value correctly.

Schneider Electric Belgium

The Write_Var instruction requires an Array of INT for the EMIS input. How do I move UINT values to a remote device?
You simply need to convert the UINT to INT with the UINT_TO_INT block and move the result to the EMIS array.
If the receiving device does not automatically see the data as UINT you would need to use the INT_TO_UINT block
to see the value correctly.