Populaire vragen (FAQ's) zoeken
Can be old control unit LUCM* from 2003 used with new base LUB32 from 2017?
Control unit LUCM* from 2003 is not compatible with power base LUB32 from 2017, because of modifications of Tesys U that were done in past.
We strongly recommend to replace at the same time the Control unit and Power base.
We strongly recommend to replace at the same time the Control unit and Power base.
Gepubliceerd voor:Schneider Electric Belgium
Ontdek meer
Productfamilie
Ontdek meer
Productfamilie