Power products including NSX and NSXm 2021 Series with Micrologic 4.1, NSX with micrologic 4/7 and Vigi add on, are not governed by residential standards such as IEC 61009 and 61008, but rather by IEC 60947-2 , annex B.
Yes they all comply with requirement of 6 mA DC current (Type A Residual current protection) as stipulated in standard IEC 60755 (that is references in IEC 60947-2).
It is written in the catalog: https://download.schneider-electric.com/files?p_enDocType=Catalog&p_File_Name=LVPED221001EN+ComPacT+NSX%26NSXm+AC++.pdf&p_Doc_Ref=NSX_NSXm_Catalog_2021
on pages B-23, B-14, B-16 and B-18.
For NSX with micrologic 4/7 it is not explicitly written, but simply these are the requirements of the IEC 60947-2 standard.