Populaire vragen (FAQ's) zoeken
Why is the EBX510 not able to connect to the ethernet network 1 from the PC?
Specific question: EBX510 Unable to connect to ethernet network 1 from PC
Reference/Material: EBX510
Test/Comments: Ethernet port 1:192.168.0.60 (configured by client) Ethernet port 2: 10.25.1.1 (default)
Client PC: Not known.
Power Led: Fixed Orange
As long as the Power LED is not solid green it will not be able to connect, it needs to wait for it to turn green
In my case I have to change my PC IP address from 10.214.17.70 to an address in the range 192.168.0.XX, e.g. 192.168.0.59:
Gepubliceerd voor:Schneider Electric Belgium
Ontdek meer
Product:
Ontdek meer
Product: