{}

Onze merken

Impact-Company-Logo-English Black-01-177x54

Welkom op de website van Schneider Electric

Welkom op onze website.
Populaire vragen (FAQ's) zoeken
Why is the RCCB not tripping when test button is pressed ?

Article available in these languages: Frans, Nederlands

Failure to trip during the test is often due to a cause that is external to the residual current device.

Measure the voltage between terminals:
a) 3 and 6 for iID
b) 4 and 6 for Vigi iC60.

This voltage must be between 85 %and 110 % of the voltage indicated on the device.

If the voltage measured is less than 85 % of that indicated on the device,the test button
may not work, although the protection device will continue to function.

If the voltage measured is more than 110 % of the voltage indicated on the
device there is a risk that the device will be destroyed.

Schneider Electric Belgium

Ontdek meer
Productfamilie
Mogelijk nuttige artikelen
Ontdek meer
Productfamilie