{}

Nossas Marcas

Impact-Company-Logo-English Black-01-177x54

Bem-vindo ao website da Schneider Electric

Bem-vindo ao nosso site.
Pesquisar perguntas frequentes
Can the AR8132A be used to replace the combination door handle of an AR3200 NetShelter SX Colocation Cabinet?
Issue:
The combination door handle on the AR3200 NetShelter Colocation enclosure needs to be replaced but the AR8132A doesn't fit.

Product Line:
NetShelter SX Colocation

Environment:
All versions and serial ranges.

Cause:
The hasp on AR8132A doesn't latch the NetShelter Colocation door correctly.

Resolution: see below


When replacing the combination lock handle of an AR3200 with an AR8132A you must reuse the hasp from the rear of the original AR3200 combination lock handle.
Do not use the hasp that ships with the AR8132A, it will not work on the AR3200.
Simply unscrew the hasp on the rear of the original AR3200 door handle and swap it for the hasp on the replacement AR8132A.
After completing this swap and installing the replacement AR8132A you will be left with the original AR3200 door handle, and the hasp that came with the replacement AR8132A.

Schneider Electric Brasil

Conheça mais
Linha:
Artigos que podem ser úteis
Conheça mais
Linha: