Issue:
Customers need to know how many 0U accessory channels are in each cabinet, and how many PDUs can mount into them.
Product Line:
NetShelter SX
Environment:
All versions and serial ranges.
Cause:
Customers need to plan installation of PDUs and cable management.
Resolution:
- All 1070 mm deep NetShelter SX cabinets have 2 0U accessory channels.
- All 1200 mm deep NetShelter SX cabinets have 4 0U accessory channels except the Networking cabinets.
- All 1200 mm deep NetShelter SX Networking cabinets (AR3340 and AR3347) have 2 0U accessory channels.
- A 1070 mm deep cabinet can mount up to 4 full height 0U PDUs.
- A 1200 mm deep cabinet (except AR3340 and AR3347) can mount up to 8 full height 0U PDUs.
- All NetShelter SX and SX Networking cabinets offer 0U accessory channels as a
Publicado para:Schneider Electric Brasil