eConversion is a patented high-efficiency mode for Schneider Electric Galaxy V Series (VS, VM, VL, VX) UPS that combines the best efficiency (up to 99%) with maximum load protection (IEC62040-3 class 1, VFI1.1.1 – equivalent to Double Conversion). eConversion typically provides a 3x reduction of the UPS electricity consumption. This live video from the lab shows an example of efficiency gain obtained when using eConversion. Discover more via eConversion Savings Calculator.
Publicado para:Schneider Electric Brasil