{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the indication of a flashing or blinking LED on the Motor Logic solid state overload relay?
Issue:
Meaning of blinking LED on Motor Logic solid state overload relay

Product line:
NEMA and Definite Purpose Contactors and Starters

Environment:
9065 Motor Logic Solid-State Overload Relays

Resolution:
The Motor Logic solid state overload relay is self-powered and is activated around 65 percent of the dial setting. When the device is powered up and activated the LED will flicker to indicate the device is monitoring the current draw.

Schneider Electric Canada