{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How do you know if you have the correct torque for the joint bolt of a I-line I busway or the joint-pak for I-line II busway?
Issue:
Torque value

Product Line:
Busway

Resolution:
The torque is correct when the outer head, of the double-headed joint bolt, twists off. If the head has been previously twisted off, torque the bolt to 70 lb-ft, +/- 10 lb-ft.

Schneider Electric Canada