{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Does a QMB324 come with bus connections?

Issue:
Characteristics of a Fusible Switch

Product Line:
QMB panelboard, switchboard with QMB distribution.

Environment:
Products sold in the United States.

Cause:
Product features.

Resolution:

Yes, the switch is complete with bus connections, but may require plug on bus extension QMB320EX depending on the panel in which it will be mounted.
The extension kits are shown on page 13-4 of the Supplemental Digest, SD177, see attached .


Schneider Electric Canada

Attachment(s)

QMB Supplemental Digest section 13.pdfQMB Supplemental Digest section 13.pdf [1.74 MB]