{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Do Schneider Electric IEC or NEMA starters meet the European standard for explosion proof enclosures?

Issue:
Is IEC or NEMA starters meet the European standard for explosion proof enclosures

Product Line:
NEMA / IEC Contactor and Starters

Environment:
North American Products

Resolution:
No. Neither the NEMA starters, nor the IEC starters offered in the US, meet the European standard for explosion proof enclosures. In other words, they are not available in NEMA 7 and 9 enclosures (commonly called "explosion proof" enclosures).

Schneider Electric Canada

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: