Search FAQs
Can I use a 3 phase surge protector in a single phase application?
Product Line:
Surge Protective Devices (SPDs)
Resolution:
No, the surge protection devices are specific to the voltages that they are rated for. It is recommended that the correct SPD is ordered for the application.
Surge Protective Devices (SPDs)
Resolution:
No, the surge protection devices are specific to the voltages that they are rated for. It is recommended that the correct SPD is ordered for the application.
Released for:Schneider Electric Canada
Explore more
Product:
Explore more
Product: