{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Does Square D offer any three phase transformers with a center tapped 240V delta secondary that will provide 120V single phase loading greater than 5% of the nameplate rated kVA capacity of the transformer? Are there any other options for obtaining great
Issue:
Does Square D offer any three phase transformers with a center tapped 240V delta secondary that will provide 120V single phase loading greater than 5% of the nameplate rated kVA capacity of the transformer?  Are there any other options for obtaining greater 120 volt load capability.

Product Line:
LV Transformers.

Environment:
Products sold in the United states.

Cause:
Product features.

Resolution:
Yes. We can design a transformer to satisfy a requirement for single phase loading of more than 5% of the rated kVA, or we can provide guidance in how to use other standard, off the shelf transformers to satisfactorily feed the load. To satisfy either case, the customer will need to provide Square D with the required loading of both the 240V and 120V loads. With this information, customers can contact Product Marketing/Support via Field Office for configuration or guidance, pricing, and lead time.


Schneider Electric Canada