{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can NEMA Size 0 8536 Melting alloy accommodate FB Thermal units?
Issue:
8536 SBO:  Can the standard melting alloy overload relay, which is furnished with a NEMA size 0 Class 8536 magnetic motor starter, accommodate the FB thermal units?

Product Line:
NEMA and Definite Purpose Contactors and Starters

Environment:
Type S NEMA Starters

Resolution:
Yes, be sure to select from the correct table for thermal units.

Schneider Electric Canada