{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Does a QO200TR provide overcurrent protection?​
Issue:
Will the QO200TR provide overcurrent protection?

Product Line:
Molded Case Switch

Environment:
Enclosed Molded Case Switch

Resolution:
No, this is a molded case switch only, with no overcurrent protection. For a similar device with overcurrent protection, consider using circuit breaker enclosure QO2TR and a QO 2 pole circuit breaker up to 60 ampere maximum. The QO2TR is suitable for use on 240Vac maximum applications only. There is no neutral assembly supplied with nor available for the QO2TR, therefore not suitable for 120/240Vac applications. The QO2TR will not accept a QO-GFI, QO-EPD or QO-AFI circuit breaker.

Schneider Electric Canada