{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
What is the maximum short circuit current rating (SCCR or AIC rating) for double throw safety switches?

Article available in these languages: Spanish

Issue:
SCCR of Double Throw safety switches

Product Line:
Safety Switches

Resolution:
The SCCR for the double throw safety switches is dependent upon the type of fuse used either inside the switch (for fusible) or protecting the switch upstream (for non-fusible).Please refer to the wiring diagram label inside the switch or the drawing of the switch for more information.

NOTE: There are some limited SCCRs for use with circuit breakers being used in conjunction with non-fusible switches.

Schneider Electric Canada

What is the maximum short circuit current rating (SCCR or AIC rating) for double throw safety switches?

Article available in these languages: Spanish

Issue:
SCCR of Double Throw safety switches

Product Line:
Safety Switches

Resolution:
The SCCR for the double throw safety switches is dependent upon the type of fuse used either inside the switch (for fusible) or protecting the switch upstream (for non-fusible). Please refer to the wiring diagram label inside the switch or the drawing of the switch for more information.

NOTE: There are some limited SCCRs for use with circuit breakers being used in conjunction with non-fusible switches.

Schneider Electric Canada
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
Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
Explore more
Range:
move-arrow-top