{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the complete overload relay replacement for a series B, size 5, 8536 SGO5 starter?
Issue:
What is the complete overload relay replacement for a series B, size 5, 8536 SGO5 starter?

Product Line:
Melting Alloy Overload Relay

Environment:
Thermal Overload Relays

Resolution:
The Series B size 5 starter utilizes a 9065SEO5 overload relay mounted onto a CT block. Order a 9065SEO5 if just the overload relay needs replacement. If the CT block also needs replacement, order # 31102-084-50. It is a 300:5 CT block. Retain any other parts from the original starter to reuse on the replacement.

Schneider Electric Canada