{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Are replacement auxiliary contacts or replacement parts available for an 8965 RO5.

Issue:
8965 RO5 Replacement parts

Product Line:
NEMA and Definite Purpose Contactors and Starters

Environment:
8965RO Hoist contactors

Resolution:
This hoist contactor is now obsolete, and so are its replacement parts. Customer will have to substitute a new Class 8965 Type RO12** with Class 9999 Type R12 auxiliary contacts for normally open or R13 for normally closed.

Schneider Electric Canada

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: