{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What size of Allen (hex head) wrench and torque is required for the wire binding screws on the 150, 200, and 225 A main lugs and main breakers used in QO and Homeline load centers?
Issue:
Product Design features

Product Line:
QO and HOM LC

Resolution:
The lugs on the main lug and main breaker load centers will use a 3/8" Allen (hex head) wrench and should be torqued to 250 lb-in.

Schneider Electric Canada