{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the Terminal Lug Data for ALL of the 200amp, US and Canada, Heavy Duty Safety Switches (for example; a HU364A, H364, CHU364, CH364, H364DS, H364AWK and CH364AWK)?

Issue:

Product Design Features

Product Line:
Heavy Dutye Safety Switch

Cause:
Terminal lug data

Resolution:
HDSS = Heavy Duty Safety Switches


The 200amp Heavy Duty Safety Switches will accept as standard (1) #6 AWG - 250 kcmil aluminum or copper conductors per phase. The Lug conductor(or wire) temperature rating is 75 degree C.
With the following exceptions:
The H225XJG and H225XJGAA will ONLY use 75 degree Copper wire and accept (1) #3 AWG - 350Kcmil. These are NOT UL listed due to inadequate wire bending space (5" for ON end and 6" for OFF end)

NOTES:
1) There is a Double lug kit available for the 200amp HDSS, BUT it is NOT UL Listed, NOT CSA Listed and is not listed on the switches wiring diagram. The Lug kit will allow for (2) #6 - 300kcmil AL/CU wires Per Phase and Neutral. The kit part number must be purchased separately for Field installation only. The kit part number is AL20DTF. The Kit contains 3 Lugs, so order 2 kits for Line and Load lugs.

2) The only UL listed alternate lugs are compression lugs, BUT they do NOT change the size or quantity of the standard wires mentioned above.



Schneider Electric Canada

Explore more
Category:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Category: