{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Is there a solid state overload relay for separate mounting for the NEMA size 6 contactor?
Issue:
Separate mounting SSOLR for NEMA size 6 availability

Product Line:
NEMA and Definite Purpose Contactors and Starters

Environment:
Class 9065 SolidState overload relays

Resolution:
There is no Square D Brand Class 9065 solid state overload for this current range however Telemecanique offers the LR9F solid state overloads that can be separate mounted for this aplication.

See page 15 of the attached catalog section for specifics and selection.

Schneider Electric Canada