{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What is the tolerance or voltage range for Definite Purpose 8910DPA coils?

Issue:
What is the minimum and maximum control voltage range of  Definite Purpose rated devices?

Product line:
NEMA Contactors and Starters

Environment:
8910 and 8911 Definite Purpose Contactors

Resolution:
Standards state that the coil must operate properly between 85 and 110 percent of the actual rated voltage or range of -15% to +10% of nominal.  Hot drop out voltage is less than 60%.

Schneider Electric Canada

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: