{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Is there an ASI-Interface module to use with XVB indicating banks?
Issue:
Identify an ASI module for XVB indicating banks

Product Line:
Harmony Type XVBC 70mm

Environment:
Signaling Units Modular Tower Lights

Resolution:
Yes, XVBC21A Base unit + cover with side cable entry. XVBC21B  Base unit + cover with bottom entry, pre-cabled (length 1 m) and fitted with M12 end connector.

Schneider Electric Canada