{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Are there any limitations in which branch circuit breakers can be mounted next to the QO2150, QO2175, QO2200 branch circuit breakers and QO2225SL subfeed lug kits?
Issue:
Product limitations

Product Line:
QO

Resolution:
Yes, due to the size of the load conductors and their exit parallel to the sidewall of the load center enclosure, certain branch circuit breaker ampacities cannot be mounted next to these branch breakers. For placing breakers below the breaker when mounted on the right side or above it when mounted on the left side, enough wire bending space would need to be available for whatever wire is being used with the breaker that is wanting to be placed next to it.

No breaker larger than 70 A can be placed across from these breakers.

Schneider Electric Canada