Search FAQs
Why is 7 1/2 HP the maximum rating that we offer for the 240V single phase 8538 combination starter?
Issue:
Is 7 1/2 HP the maximum rating that we offer for the 240V single phase 8538 combo starters?
Product Line:
NEMA Contactors and Starters
Environment:
Class 8538 Combination Starters
Resolution:
The applicable NEMA category definition does not include or recognize anything above 7 1/2 HP for 240 volt single phase.
Customer will have to size by the full load current.
Is 7 1/2 HP the maximum rating that we offer for the 240V single phase 8538 combo starters?
Product Line:
NEMA Contactors and Starters
Environment:
Class 8538 Combination Starters
Resolution:
The applicable NEMA category definition does not include or recognize anything above 7 1/2 HP for 240 volt single phase.
Customer will have to size by the full load current.
Released for:Schneider Electric Canada
Explore more
Range:
Explore more
Range: